This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL082: 我在使用Multisum仿真三相交流电输入电路的时候发现,两种不同的运放仿真结果不一样

Part Number: TL082
Other Parts Discussed in Thread: LM324,

运放TL082的VCC-接GND,VCC+接9V  运放LM324运放的电源接法和TL082一样 为什么LM324的输出波形是正弦波而TL082仿真电路却是不规则的波?

谢谢!

  • 您好,

    单电源9V供电这两种运放都可以这样接,但是它们的输入和输入范围不一样,如果超出了它们的输入或输出范围,运放就会工作在非线性区,输出就会异常。

    TL082您具体使用的是哪个型号?后缀是H还是M或C还是其他哪个型号?看下输入和输出信号是否满足其输入输出范围?

  • 您说的输入范围是运放两个输入的差值还是指其他?

  • 如上数据表截图,TL082H的输入信号范围是(VCC–) + 2V  ~  (VCC+) + 0.1V ,如果单电源9V供电的话,即是2V ~9.1V

    其他后缀的型号,输入信号范围是VCC– + 4V ~ VCC+ – 4V,如果单电源9V供电的话,即是4 V ~5V。

  • 如果未解决您的问题,请回复帖子

x 出现错误。请重试或与管理员联系。