This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM358: LM358运放作比较器使用,输出受限于供电电压

Part Number: LM358


您好:

         如第一张图所示,我想使用U1B LM358作为比较器使用,其供电电压5V,5PIN正向输入电压为3.6V,6PIN反向输出端电压为1.78V,按照第二张和第三张的理解:V+>V-时Vout=V+,A为开路增益,按这样的增益,其应该无损失的方法,但7PIN的Vout为3.8V左右,(R11上拉去掉或保存不影响其LM358输出结果为了),为什么是3.8V?当我VCC从5V调到6V,其他什么都没动,输出就变成4.8V左右了,我使用PSPICE仿真,试着给供电电压不同范围时,±15V,±10V,其Vout发生变化,我想知道为什么输出受限于供电电压,开路时不应该增益很大?希望您能回答一下