This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LF353: 型号替换

Part Number: LF353
Other Parts Discussed in Thread: OPA2991, TLV9362, TLV9162, LM6142, OPA2725

目前使用LF353做PI调节,±5V和5V单电源供电都有,发现此时输出电压最大只能在4.1V附近,想问下TI是否有型号可以pin to pin替换LF353 

供电可以兼容±5V和5V单电源供电,最大输出电压峰值最好能够达到5V,然后slew rate>13V/us