This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA333: STC8H采集仪表放大器INA333的放大信号遇到点问题

Part Number: INA333
Other Parts Discussed in Thread: INA133

电阻桥测电阻的微小变化,经INA333放大20倍,放大后的信号不是个稳定值,也不像是干扰,请看下图,不知道哪里没对,难道是没加输出隔离?第一张图是原理图,VResIn就是进STC8H ADC口的信号,第二张图是这个信号的示波器图

  • 您好,INA333的同相输入端IN+接的VoutA 接到哪里了?VCCA 是多大电压?

  • VoutA和地之间,会接入一个电阻,目的就是测这个电阻的大小,量程50欧。VCCA的在我的设计中直接1S锂电池供压,会用2.5V的精准电压来标定它的大小。

  • 我把图中的0.1uF,换成20uF后,放大器输出示波器上就只是稍有波动了,并且值就是小电阻对应产生的电压差。但我不知道的原因

  • 电源这里的0.1uF没问题,你指的Vout接地的这个0.1uF电容吗?这里相当于容性负载,容性负载会影响运放的稳定性。

    INA133的容性负载能力只有500pF,建议将C17去掉再测下波形是否正常。

  • 去掉就对了,谢谢,受教了

x 出现错误。请重试或与管理员联系。