Other Parts Discussed in Thread: OPA380, LM2663
opa380的正输入的偏置电压必须是0.5v吗?
可不可以用+/-2.5v供电?
0.5v的偏置电压怎么产生?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您说0.5V偏置指的是datasheet中一个线路里提到的吧?那个仅仅是一个特例,可以调整输出范围从0.5V开始,您可以根据自己的需要来改变。
供电方面当然可以采用双电源供电,当然如果想在单电源下使输出达到0或者轻微的below ground可以采用输出接下拉电阻。
您好,我用opa380接的是光电探测器,探测器的输出电流信号是正弦波,有正有负,单电源时只有正半周期,用正负2.5v是不是就可以,正负都有?
谢谢
请问opa380正常工作时的电流有多大?
LM1117-2.5产生2.5v,LM2663产生-2.5v 供电可以吗
楼主你好
1、请问opa380正常工作时的电流有多大?
opa380 Quiescent Current 为7.5mA,加上输出驱动电流即为总消耗电流。
2、LM1117-2.5产生2.5v,LM2663产生-2.5v 供电可以吗?
可以