Other Parts Discussed in Thread: LMV358
进入运放的信号时正弦波,出来之后峰顶就出现了第一张图所示的那样的波形,第二张图是电路图,供电是7805,电位器是200k的,进入的信号峰峰值20mv左右,请大家看看是哪里出了问题。谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LMV358
进入运放的信号时正弦波,出来之后峰顶就出现了第一张图所示的那样的波形,第二张图是电路图,供电是7805,电位器是200k的,进入的信号峰峰值20mv左右,请大家看看是哪里出了问题。谢谢。
我初学运放,大二了,有很多不明白的地方,带宽增益积是在不同的频率下运放对信号的增益,20khz时的增益石30db多,对于5v供电的线性区已经足够了啊,是不是我理解上有不对的地方,sr参数主要是正弦波现成三角波,实际上看输出波形没有很大的变化,出来的信号还是正弦波,输出信号是给单片机的ad,输入信号的幅值是20mv,mv358的输入失调电压最大是10mv,还有一个是相位裕度,一直没明白是怎么回事,是您说的裕度小么,还是说这颗运放对于现在的输入信号没有很好的处理。麻烦您给解答一下,谢谢。
输入信号的频率是固定的20khz,频率正负2khz,
输出信号的幅值就是从供电的地到5v,一般最大会调整到4.5v左右,信号的幅值会随输入信号的幅值变化,
1、Slew rate 是压摆率,顾名思义就是 信号斜率, dV/dt, 根信号类型没有关系,我们一般以正弦或者方波作为测量信号。
对于正弦信号: slew rate 应该大于 2* pi * f * Vom,f 是正弦信号的频率。
LMV358 SR 是 1V/us,SR > 6.28 * f * 2.5. f < 63khz.
两个表述的建议:
1、建议楼主把问题分点描述,这样方便大家阅读,整篇描述看的也很费劲,另外就是表述逻辑的因果性;
2、配图请说明一下,哪个描述对应哪个波形;
几点问题:
1、从图片看,没有看到楼主说的毛刺,没有看到波形有什么问题,楼主能否标示下?
2、信号源是什么,是传感器还是信号发生器?