Other Parts Discussed in Thread: OPA2228, OPA228, OPA227, OPA637
我使用OPA2228双运放,其中一个运放做THS5651的输出I-V转换,将该电压信号经过电阻分压衰减送进另一个运放组成的射极跟随器,但是测到在进入分压前没有问题,但是在分压之后的一点信号就出现了失真,请问是什么原因,如何解决?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
什么是适合增益小于5的运放,从哪些参数可以看出,如果是I-V转换,那么增益又是如何算?谢谢
我用Pspice仿真,在200mV,200kHz波形正常,而增加射随器的输入电压或者信号的频率,波形会变得不稳定出现杂波,请问这是什么原因
1、市面上有一些运算放大器是没有经过完全补偿的,目的是为了拓展带宽的应用。例如op37 opa228 opa637等等。这些运放不能工作在单位增益下,即G = 1。一般会对最小增益有要求,例如 G > 5 , G > 10。
2、 I-V变化也是一样,将电流源 的 内阻考虑 进来, G = - Rf / Rio, 其中,Rf 为 反馈电阻, Rio 为电流源输出阻抗。
Q:我用Pspice仿真,在200mV,200kHz波形正常,而增加射随器的输入电压或者信号的频率,波形会变得不稳定出现杂波,请问这是什么原因
A:楼主请看之前为您大概仿真的结果。具体就是前面说的因为OPA228并不是单位增益稳定放大器,所以输出就会出现不稳定,无规律的震荡。非单位增益稳定放大器比较适用于I-V转换,因为未加补偿所以具有更好的带宽,SR更快。要做跟随器的运放必须要求单位增益稳定,也就是上面截图给您的关于OPA227的"Unity-gain stable” 这个描述。 属于Unity-gain stable的器件一般会在datasheet 中写明。楼主可以继续用OPA228做I-V,另外用227做跟随。