This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助,稳压负反馈电路为什么输出电压不够

网友  xiao2_son 在21ic 模拟技术 论坛问以下问题, 长期未解决:

如图,稳压负反馈电路输出电压不够,R1左边的输入是0~5v,经过运放放大5倍然后输出,R4我是用可调电阻代替,虽然说输入输出线性关系不是很好,但是还是差不多5倍这样子,图里面的30V我是根据R1边的输入慢慢增大的,当R1边的输入从3.5v左右开始增大时,输出就在不到19v的位置停了,我让输入为4v,30v的位置从20v加到30v,输出还是不到19v,这样解决这个问题?这个图仿真输出的可以达到25v的,怎么办?求助!!

  • 楼主你好!

    请问你的实际电路中,非线性的点最开始出现在哪里?

    1、是第一个运放输出、还是第二个运放输出?

    2、另外,输出刚到达19V的时候,运放输出电压是多少?

    3、另外,BJT是电流控制器件,不是电压控制器件,这根楼主选择的NPN管的β值有关。