Part Number: THS4541
Other Parts Discussed in Thread: LMH6555
想用THS4541作为ADC的前端的驱动电路。
THS4541的Vos是0.45mV,我需要测的电压最小值非常小,可能会小到0.5mV。这样的话THS4541还能用吗,有办法可以补偿Vos吗,还是说必须选用更小Vos的放大器?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
您的有用信号可能会小到0.5mV,这里的0.5mV是交流信号还是直流信号?如果是频率比较高的交流信号,且不关心被测信号中的直流成分,您可以增加交流耦合电路将失调电压消除;
THS4541的Vos在TA = 25°C时最大是±0.45mV,加上温漂失调电压会更大,因此如果有用信号为0.5mV的话,在输出信号中有可能无法识别出有用信号;因此需要选择Vos小于被测信号的运放,或者通过增加调零电路消除失调电压的影响;
在LMH6555 数据表Figure 31 ~ Figure 33有失调调整示例,您可以参考;
下面链接文档希望对您设计电路有参考价值:
https://www.ti.com/lit/an/sboa332/sboa332.pdf