Part Number: INA296A
Other Parts Discussed in Thread: OPA365, THS4541
你好,我看到电流检测放大器的带宽范围最大只能到1300KHz。有什么办法能测到电流中更高频的成分吗,比如5MHz?
还有,后面ADC是差分输入,我是不是还需要在电流检测放大器后面加一级全差分运放来转差分?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,是的,电流检测放大器的最大带宽为1.3Mhz,5Mhz的话电流检测放大器是不够的,并且最大1.3Mhz的电流检测是单向的。您的理解是对的,如果ADC需要差分输入的话,需要通过全差分运放来转化为差分输出。
您好,如果检测较大带宽的信号,一种方案使用这种电流放大的多级放大,使用小增益增加器件数量,增加感应电阻,如果使用较大感应电阻,那么会引入噪声,增加功耗导致接地干扰。另一种方案就是使用单个高速放大器,宽带宽,使用较小感应电阻实现单个器件的高增益。对于电流感应放大,就像您说的,确实需要选择低输入失调电压和低输入噪声电压的器件,比如可以参考OPA365,它在100Khz的时候输入电压噪声为4.5nV/√Hz,典型失调电压为100uV。