This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA365: 电流采样问题

Part Number: OPA365
Other Parts Discussed in Thread: OPA376, LM7171

 您好,最近遇到了运放电流采样的相关问题。我按照如图所示的电流采样电路进行电流采样,,我想取得100K-200K的高频成分同时还需要直流分量。相同的电路分别使用了两种运放,分别是OPA376和OPA365,测试波形如图所示。不知道为什么OPA365的带宽要高很多但是波形如此失真?

  • 您好,

    所需要采样电流直流分量是多少?交流分量是多少?被采样电流回路是否与运放共地?您 可以画出被采样电流回路的示意图吗?运放供电电压是多少?因为您这个电路不是标准的差分电路,我想用TINA做下仿真

  • 您好感谢回复。 直流分量是0-42A,交流分量是峰峰值20A。被采样电流回路与运放共地。Vcc是3.3V。因为直流分量是0A的时候,交流分量有负值,所以要加入了一点偏置。

  • 今天用了别的运放LM7171,发现也是OPA365这样的情况。最后分析发现是放大倍数过大,导致失真。OPA376之所以是三角波,是因为OPA376的压摆率低,也是一种失真的现象。当把两个运放放大倍都数降低到10倍以后。波形如图所示。他们输出都出现削顶失真,现在是这个削顶失真不知道是怎么回事儿?

  • 我想了解的是这个电流是怎样产生的,电流回路中是否有除采样电阻外其他的负载?采样电阻两端的电压是多少?最好可以给出被采样电流回路的示意图;

    0.3mΩ的采样电阻,交流电峰峰值是20A,那么采样电阻的电压就是6mV,可以用示波器测量出来,您可以给出采样电阻两端的电压波形吗?