Other Parts Discussed in Thread: LM675
请教大家一个问题,这个电路中如果RX1大于5K时,输入信号为20KHz,输出信号的波峰和波谷会添加4MHz的信号。随着RX1的增大,输出信号如示波器所示。为什么会出
现这个问题,请高手给讲解一下,非常感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
RK越大增益越小,在无补偿情况下LM675适合用于gain=10 or higher的应用。
请先尝试去掉C18,较小的电容来补偿反馈以获得平坦较为响应曲线是可取的,但是一个大电容会造成曲线不平坦。反馈路径上的电容使得高频部分的频率响应曲线变得不平坦。在稳定性涉及到单位增益的高频部分,这个电容可以视为短路。
楼主您好,
在增益低时,发生自激是这个电路的固有缺点,不是LM675芯片的问题。
请参之前的一个帖子:
http://www.deyisupport.com/question_answer/analog/amplifiers/f/52/t/22940.aspx