Part Number: THS3491
Other Parts Discussed in Thread: THS4031
请问各位大佬,现有一个±2.5v的46Mhz的模拟电压方波,现在需要将其抬升到0-5v:
1、用同相放大器的设计思路该电路为何会出现以下报错。
2、该电路还有什么需要完善和改进的地方吗,如果想要较好的效果。
万分感谢!!!!!



This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,VCC和VEE电压反了,按照标记都是5V的话,正负极接反了。另外,您直接使用了5V电源的话,上面接GND即可。 您把您的.TSC电路附上我看下,VREF接的J1接的是什么?

谢谢您!我的J1没有接,因为不太清楚其工作机制应该如何计算,请问方便加个联系qq或者邮箱吗,我把文件发给您,实在麻烦了,这个电路较为重要且加急,万分感谢您了!!!!!!
您好,是不方便发在这里吗?如果J2悬空,那我按照您的电路搭建一个相同的仿真试试。
另外,关于您的应用,另外,THS3491的供电电压最低+-7V,最高+-16V。所以仿真电路中您采用的+-5V也是不合理的。 它是一款电流反馈运放,电流反馈运放为了其稳定性,反馈阻值一般选择datasheet中推荐的阻值。
所以我建议您更换其他电压反馈的运放,目前要求是不是+-2.5V正弦输入,46Mhz,需要输出0~5V的这样一个需求?
是的是的,是这样的需求,只不过是方波输入,供电电压可以±12v或者您定义的合理值都可以的,小问题,主要看波形效果和电压幅值。麻烦您了
您好,仿真文件没看到呢,点击插入-图像/视频/文件--上传就可以了。
另外,如果是只是需要+-2.5V的信号变为0~5V输出,可以直接使用我们的差分放大器,Vout=(V+)-(Vin-)。
其中Vin+=2.5V, Vin-=+-2.5V输入。输出即为0~5V波形,设计起来非常简单。
不好意思,我刚看了下差分放大器的带宽,本来想TINA仿真一下,结果看差分放大器的带宽都比骄小,小信号带宽最大5Mhz,所以不满足您的应用。
我用THS4031试了试,这个是6Mhz的信号仿真结果,因为运放的SR特性,所以输出不可能是绝对的方波。 但是46Mhz的信号的话,输出有些失真。

下面是46Mhz的方波输入,可以看出输出是有些失真,这是因为4031的SR不够,SR=2*pai*f*Vp=2*3.14*46M*2.5=727V/us.
所以我们在选择带宽时,不仅需要带宽够的,还要考虑SR的影响。
忘记附上46Mhz,SR不够的情况下的输出失真,可以参考下,选择带宽够,SR够的高速运放去实现您的应用。

您好,我上传在这里啦,我所选的THS3491就是考虑了带宽和供电电压两个因素综合考量的,麻烦您帮忙参考一下看看~~
您好我看了下附件TSC文件,问题比较多,PD_OUT为低的时候,输出disable,所以此引脚需要拉高。另外您的电源设置的也不太合理。
我用THS3491重新搭建了下,您参考下附件。这个是46Mhz下的仿真,由于THS3491是电流反馈为了保证其稳定性,所以Rf的值我们尽量使用datasheet中给定的参考值。

我这个电路其实就是一个单位增益缓冲器,然后在+-2.5V的输入信号上叠加了一个2.5V的偏置电压,那么运放的输入端就抬高到0~5V了,然后单位增益,输出也是0~5V。


您好,在您的指教下,我现在敲定用THS3491DDA这一款芯片了,但有两个问题要请教您:
1、您的电路按照datesheet来说,是否应该是RF=798,我仿真了一下,确实对于方波来说,效果会更好一些。附上现在的文件,以及想请教这个电压过冲如何消除或改善,求大佬指点。
2、原本的同相放大电路,我的修改了供电和PD_out仍报错,运行出错误波形,我不太确定是不是因为我没有按照您那样把供电电源单独设置,而是直接连接在电路里,我也一并上传 ,麻烦您帮忙指点一下,谢谢!!2376.THS3491.TSCTHS3491_zengyi.TSC
您好,您的TINA中电压极性接反了,我给修正过来了,已经不报错了,但是输出是直流约3.44V。您看下我把电压极性改过来的TSC文件你看下。