如上图中黄色部分,这颗料是单5V供电的,数据手册中这三项参数不是很理解。
另外测试不相关的交流信号,如下图方式,将对地信号限制在0-2V范围内,没什么大毛病吧?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如上图中黄色部分,这颗料是单5V供电的,数据手册中这三项参数不是很理解。
另外测试不相关的交流信号,如下图方式,将对地信号限制在0-2V范围内,没什么大毛病吧?

您好,
7.3 Recommended Operating Conditions 章节中这个表格中的参数是推荐的工作参数,Absolute input voltage,是任何瞬间都不能超过的VIN输入范围,在数据表7.1有绝对最大额定值,在7.1表格中VIN的范围是GND1 – 6V ~ VDD1 + 0.5V,超过这个范围设备就会永久性损坏,7.3表格中VIN范围是–2V ~ VDD1,是推荐的或建议的不允许超过的范围,对VIN输入造成设备损坏的范围留有一定的裕量;
VFSR 是线性输入电压范围,超过这个范围,电压就不再线性输出;AMC1311的增益是1,VOUT=VIN,若VIN超过–0.1V ~ 2V这个范围,输出就不满足VOUT=VIN;
VClipping,是2.516V,VIN超过这个电压,输出就会削顶;AMC1311输出行为如下图48截图所示:

VIN输入信号在0-2V范围内没问题,但需注意是以AMC1311的GND1为参考点;