This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM386的增益怎么计算的啊?(根据它的内部结构分析)



在2管脚接地,从3脚输入,1、8脚不接电阻电容,7脚接电容到地时,怎么计算它的增益呢???

给出的是Avf=2R7/(R5+R6),但我就是一直算不出这个结果,求高手指教

  • 有反馈吗?其他引脚呢?能否把实际的电路图贴一下,文字描述理解可能会有歧义。

  • LM38*系列这样的构成属于典型的功率放大。R7右边部分作为互补对称输出级并由电流源和T8/T9组成的等效PNP提高放大倍数。R3,R4,R7分别提供差分输入的静态工作电流,并且对称,即大小相等,此刻R5/R6并没有直流电通路。关于放大倍数的计算其实需要知道这里引入的反馈有直流反馈和交流反馈,这是以前书本上都有讲到的。直流反馈就是简单的将Vo引到T4,作为静态工作电流的同时保证Vo的稳定。交流反馈即将R5/R6看做一整体,由于对称将它们的中间点看做交流电的参考点位(并不是PIN 8),然后通过这个参考点位,结合Vo和PIN 3(+输入极)看做一个电压反馈网络,则反馈系数F=((R5+R6)/2) / (R7+(R5+R6)/2)  则根据基本反馈理论A≈1+R7/((R5+R6)/2)≈21

  • 哦哦   太感谢了,之前忙着考试,没有注意看帖,原来一直把参考点看错了,所以一直算出来都是少了一个2倍的结果