Other Parts Discussed in Thread: OPA180
我现在想将一个FPGA发出的1MHz,0~3.3V的方波信号放大到0~10V,请问有合适的电路参考吗?OPA820手册附带的参考差分放大电路,能满足我的频率条件吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,从带宽和压摆率的角度来看,OPA180都满足您的需求。
但是从电压来看,+-5V供电的话,输出电压swing为+-3.7V,那+-5V供电,0~3.3V 输入,正向电压最高达到3.7V。
因为OPA180 不是轨至轨输入和输出的,所以单电源供电的话,靠近0V输入的信号也是无法处理的。
所以要选一款宽供电电压范围的运放。
您好,不好意思我打错型号了,我所说的是OPA820,不是OPA180哈 。
选择运放时候,我们需要考虑它的增益带宽积,压摆率,供电电压,输入输出电压范围。如果这些都满足,就可以实现。
比如0~3.3V输入,那尽量选择双电源供电,因为很多单电源供电的运放如果不是轨至轨的话,对0V附近的信号是没法处理的,所以建议选择双电源供电。 其次就是看如果需要5V输出,供电电压至少需要多少,比如输出电压幅值为(V+)-1.3V,那么如果输出5V,至少需要6.3V的电压。
其次就是0~3.3V输入,0~5V输出,增益大概在1.52左右,所以在实际选择Rf和Rg的常用阻值时可能很难做到精确的这个增益,所以只能说大概输出0~5V。