This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好, THS3091的供电电压范围为+-5V~+-15V,单电源的话为10V~30V,但是由于它不是轨至轨输入输出,所以是达不到输出30V电源轨的。
和您确认下,输入信号是0~3.33V方波信号,输出0~20V或0~30V的信号是吗?
您好,2Mhz,放大倍数约为9.09,增益带宽积至少20Mhz以上,如果选择高速运放(>50Mhz). 单电源供电的话没有输入轨至轨的,因为您要处理0~3.3V信号,0V信号是无法处理的。双电源供电的话,最大供电电压为44V只有一款LMP8672,即+-22V,所以达不到输出30V 的幅值. 并且我仿真了下带宽不够,2Mhz的时候是不能正常线性输出的。
抛开高速运放,在通用运放里,选择宽电压工作范围,输入能轨至轨V-的LM7372,并且单电源供电输出是能达到30V的,但是 20Mhz的带宽,同样当信号为2Mhz时,不能线性输出。
这两个仿真我都是以100Khz为例,可以看到是正常工作的。
所以如果必须能处理0V附近的信号,2Mhz放大约十倍,要同时满足GBW,轨至轨输入输出(因为输出20~30V的的这个需要宽电压工作范围)的话不太好找。
还是要考虑高速运放,选择THS3491,如果对称正负电压供电最大只能到+-16V,所以可以考虑不对称,即正压Vcc=28V,负压Vee=-4V。保证不超过32V的供电电压。
还是Gain=9.07,可以看到输出稍微有些削顶失真。
如果考虑输出20V的话,gain=6左右,由于THS3491是电流反馈,我们在选择Rf的时候尽量选择datasheet中推荐的值,然后根据增益去匹配Rg的值,参考datasheet Table2不同增益下的Rf和Rg的取值。可以看到是没问题的:
方波仿真如下,同样也是Gain=6,幅值20V的信号,但是我们要知道运放受压摆率的影响,可能不能完全做到方波的效果但是由于THS3491是高速运放,可以看到输出几乎还是方波,斜率还是比较陡峭的:
您好,高速运放很少有输入轨至轨V-的,所以如果单电源供电,是很难 处理0V附近的信号。
所以我选用的是不对称双电源供电,V+=28V, V-=-4V保证最大不超过32V电压。
您指的功率被放大,和您解释的是,负载不同,输出幅值有不同。 我仿真的是在没有接负载的条件下测试的。