This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM7171: 是否有过压过流保护

Part Number: LM7171


我在使用LM7171搭建电压反馈放大电路时,反馈系数为2,输入正弦波电压10V,输出饱和,运算放大器会损坏嘛,它内部有过压和过流保护嘛。最大能承受的输入电压多大

  • 您好,

    输入电压范围与供电电压有关,在±15V供电时,输入范围是±13.35V(查看 datasheet 6.5 部分  ±15V DC Electrical Characteristics );在±5V供电时,输入范围是±3.2V(查看datasheet 6.7 ±5V DC Electrical Characteristics);

    您上述应用中LM7171的供电电压是多少?LM7171 是一款比较老的器件了,在LM7171 datasheet中,仅给出了±15V供电时的 差分输入范围,没有给出单端输入范围,也没有说明是否有保护电路,但是建议按datasheet中给出的共模输入电压范围来使用LM7171 ,即输入范围不要超过供电电压±VS-2V

  • 我是15V供电的,不过我给的输入有些时候可能会超过15V,我想知道如果超过了限值,运放里面是否有保护电路,后面还能用嘛,还是说运放直接就损坏了。

  • 我在内网看到有美国的工程师说 LM7171输入端对Vcc和Vee有二极管,当二极管两端电压超过0.3V时,这个二极管就会导通,如果通过二极管的电流很大(超过±10mA),则可能永久损坏设备。 如果施加的电压有足够的电流限制(+/-10mA或更低),则不会发生损坏。
    因此,如果电流限制为小于10mA,则不会有损坏设备;