Other Parts Discussed in Thread: TAS5611, OPA1632
我们正在用TI的TAS5611+OPA1632方案,调试样机中发现,TAS5611输出功率略小,可否调整功放芯片前面的OPA1632运放的放大倍数来改善,如能调节,请告知调节方法,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
关于您的这个问题,我们几个工程师最近研究了以下,得到下面几个结论: 因为TAS5611的输出功率是和PVDD,THD+N,系统效率以及负载大小有关的,提高TAS5611输出功率的方法,首先要考虑的是PVDD,最好采用效率比较高的DC-DC 电源32.5V,防止静态电流过大增加功耗,另外需要考虑的就是PCB布线,比如power端的去耦电容要求尽量靠近芯片端,走线尽量短,power走线要尽量宽等这些也是影响效率的一个因素。最后一个原因,请检查电路中是否有负载端接的线绕电感导致静态电流过大。
确实是电压稍低的原因,因为看规格书上有写TAS5611可以工作在16-34V,我们就用了24V的开关电源,现换成32V,功率立马就上来了,谢谢TI工程师,你们辛苦了。