我们使用LMH6518作为VGA,发现在不同的信号功率下,LMH6518的输出输出端P和N的共模电压差距很大,P端可能只有1.1V,N端会有1.3V,请问这个情况是什么原因呢?我的ADC输入共模电平是1.2V,所以6518的输出端我只串联了0欧姆电阻直接到ADC,此时,ADC采用有符号数输出,ADC的采集结果只会出现低于0以下的符号数。请问这是怎么回事儿呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们使用LMH6518作为VGA,发现在不同的信号功率下,LMH6518的输出输出端P和N的共模电压差距很大,P端可能只有1.1V,N端会有1.3V,请问这个情况是什么原因呢?我的ADC输入共模电平是1.2V,所以6518的输出端我只串联了0欧姆电阻直接到ADC,此时,ADC采用有符号数输出,ADC的采集结果只会出现低于0以下的符号数。请问这是怎么回事儿呢?
您好,能否附上LMH6518的电路看下?
输入信号幅值多少,增益多少?您这里指的P端1.1V和N端1.3V分别是P,N的共模电压,还是P端和N端的输出幅值?因为按照共模电压的定义,Vcm=【(Vout+)+(Vout-)】/2,所以(1..3+1.1)/2=1.2V是没问题的。
上述是原理图,输入端N端的共模电压为2.5V,输入端P和N端的直流偏置电压差会有将近60mV的差异,前述问题中的输出P端1.1V是指直流偏置,并且,输出P端和N端的直流偏置会随之输入信号的变化而变化,同时,Preamp选择LG和HG也会对输出端的直流偏置产生影响。请问只是什么原因引起的呢?
说明一下,我后端接的是ADC,所以LMH6518的输出共模脚是和后端ADC的VCM脚连在一起的,ADC的差分阻抗是100Ω,所以LMH6518的输出端只是接了0Ω电阻。
输入端N端的共模电压为2.5V,输入端P和N端的直流偏置电压差会有将近60mV的差异,
您好,您是采用的单端输入吗?输入幅值范围为多少?
因为根据您的这句描述,不能判断您的输入信号幅值范围是多少,LMH6518前端是全差分运放,输入差分输出也是差分,如果您是差分输入,因为运放放大的是差模电压,所以共模电压为零,如果您是单端输入,是P端输入信号吗?N端的2.5V共模电压是什么?
如果有输入信号的波形也可以附上。
P端幅值是1Vpp以内的信号,频率的话从DC到500M,LMH6518的带宽全开
那输入没问题,频率的话从DC到大于500Mhz~800Mhz的时域性能都不会受到影响。
电路也没什么问题,辅助输出通道AUX CH2是否通过寄存器将其disable掉?建议将其disable,验证输出是否还是不稳定?