This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRF37D73: 我输入的信号是640MHz~680MHz之间的频率,放大器没有放大的问题?

Part Number: TRF37D73

各位师傅好,请教一下,

1、我使用TRF37d73芯片来对话筒信号进行发射功率放大,频率范围为640MHz~680MHz之间的频率,但是我发现放大器并没有放大作用

2、芯片供电电压是3V

请师傅协助解决,万分感谢

  • 您好,

    TRF37D73的输入源和输出负载都必须是50Ω,以匹配 TRF37D73内部的阻抗,否则的话会发生反射,使得功率无法实现最大传输 ;

    另外,可以附上原理图吗?检查下原理图,下面是EVM原理图,您可以参考,其中对于TRF37D73,R2=0Ω