我用TPA3112D1 按芯片的技术手figure 17的样子连的电路但是输入 给的是电脑音频口出来的音频信号可是输出没有变化的波形,而且SD 脚一直为低为什么????
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Yi Lin,
请将你的完整电路及PCB版图发上来。输出滤波器使用的是磁珠还是电感?PVDD供电电压是多少?喇叭阻抗多大?
SD引脚有无外部控制?是否和FAULT引脚一起短接上拉至PVDD?
若SD引脚与FAULT短接并上拉,一直为低说明电路输出有短路或触发了直流检测,导致FAULT引脚置低报错。麻烦你仔细检查一下PCB及电路,另外建议你再参照我们的EVM板原理图及PCB Layout进行电路设计,需要注意的是若你的PVDD上电速率高于10V/ms,14引脚必须串接100kΩ电阻。
Thanks.
Jacky Wang,
您好!我是华力电子(惠州)有限公司王工,我们新开发的一款音箱正要使用TPA3112D1,请求把您们的EVM板原理图及PCB Layout发到我邮箱wyr_cctv@126.com,不胜感激!
Thanks.
JACKY WANG,
您好,请帮忙发TPA3112D1的EVM板原理图及PCB Layout电路设计给我参考,谢谢!我的邮箱wyr_cctv@126.com,辛苦了,请帮忙!