Other Parts Discussed in Thread: LOG114, LOG2112, LOG112, OPA2333
焊了两块板。 Vref正常2.5V。 电压正常正负5v 。就是接了PD后无论输入多少都没反应。帮忙看看。
激光器接到PD上,让PD产生电流。 这些地方都检查没有问题。 无论pd正反放都无反应。电阻选择2.5M和5M都试过。
这种最简单电路都没反应。。。没招了。 不知道我在I2这个脚上接PD行不行?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
lven:
谢谢你的回复。今天我又做下试验。
1.调节ref上的电阻到2.5M 串了一个keithley的电流表测 ,调节到1ua。
2.将电流表串接到PD和log114的输入之间,得出如下数据:(注,光源输入有一个1分2,另外一头接光功率计以便观察。小数点后大概忽略)
光功率-20db左右时, 电流表显示10ua,logout是1v,后面狂跳。 计算应该是。0.375v左右吧?
其他就不用说了, -17db 20ua时 就已经是3.35v, 跳动是10好几个mv。。。晕死。
是不是我I1 和 I2 接反了? 即时接反了,发现跳动也太厉害了。。。
望指教
我仔细看了下原理图,就这么简单的三根线。然后我吧I2 和 I1 互换了下。。也就是PD接I1 ref接电阻接I1,完全按照datasheet上来得到以下一组数据。
pd power Vlogout [note1] vlogout I2[note2] the correct result must be.
(test by power meter) (PD directly connet with I2) ( PD-keithley 486-I2)
-10.147dBm 0.75 0.75v 100.38ua 0.75V right
-19dBm 0.375 0.375 10.01ua 0.375V right
-30.18dBm 0 v 0mv 1ua 0v right
-39.833dBm -2v -2v 101na - 0.375V
可以看到 pd电流大于1ua ,时 输出基本可以认为正常。但是一到小于1ua就不正常了。变化非常大。100na时基本就到了-2V,按公式应该是
-0.375才对,应该是基本对称的啊。??求帮助。
when the I1 < 1ua, the voltage out is incorrect. what's the problem??
这个电流非常重要,是一个参考。两路的话,建议用个低噪声的运放,想OPA2333,分成两路,分别通过电阻接到IA和IB里去