This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. 尖峰频率150Hz,怀疑是50Hz市电的3次谐波干扰。把C8改大一些,比如改成30nF,则R20/C8这个低通滤波器决定的3dB频率是86Hz,对150Hz的干扰多多少少能有一点抑制。
2. 电路的直流工作点很奇怪。先是用R21和R22分基准,然后用U5A放大直流信号,然后不加处理直接送到U4A,不清楚这样的用法是否可靠。
3. 为什么要加R38?
1.可编程直流电源加电后会出现干扰,但是线性光耦前端没有干扰,干扰出现在线性光耦后端。另外86Hz的频率几乎把要分析的信号滤的干干净净,我想分析至少10k的频谱
2.第二点不是很明白
3.线性光耦是靠电流匹配的,加电阻R38形成电流通路进而对电压进行跟随送入到AD
1. 加“强电”之后输入端POWEROUT也没有那种150Hz的尖刺?确认一下。然后再确认一下加强电的时候,强电会不会影响板上电源+/-15V,M5V。
2. 分析直流共模时,输入POWEROUT置零,即接地。直流共模信号REF5先经过R22/R21的分压,然后经过R23/R24/U5A的5倍同相放大,再经U4B的buffer到达U4A。请确认这样做是否可靠。
工程师,针对之前的电路,我想咨询下该电路是不是不能检测到电路电流信号中的mV级的交流分量(可理解为毛刺),因为电流(叠加了交流分量的直流分量5A电流)经过10mΩ的检测电阻后变为了mV级电压,若交流分量峰峰值为200mV,此时就只有2mV,该量经过LM358是不是不准呢?看到网上说LM358的失调电压就3mV了
5A直流电流经过10m Ohm电阻,变成50mV直流电压,2mV是怎么计算的?
如果信号2mV,运放的offset有3mV,那确实有可能offset会把信号淹没。
电路发生故障时在电流上会产生200mV左右的毛刺,那么在检测电阻上的体现就是2mV
"电路发生故障时在电流上会产生200mV左右的毛刺,那么在检测电阻上的体现就是2mV",是200mA左右的毛刺经过10m Ohm电阻转化成电压吧?
LM258的offset典型值3mV,比想要检测的2mV电压值还大,这个运放不适合你的应用。可以考虑用一个低offset的运放,比如OPA376或OPA2376。
1.确认加强电后输入端POWEROUT、电源15V、M5V电源均没有毛刺,但光耦输出端7脚仍有毛刺
2.我检查到光耦输出端7脚与R38之间的距离达到1.6cm,请问这根信号线这么长的长度是否会产生这样的干扰?