查看AFE031文档SBOA130A和SBOS531D时发现两个文档中对于设计参考电路中的电容关于C8的计算公式不一样,一个是计算公式分母中含的是20K欧,另一个是分母中含的2K欧,整整差了10倍,很疑惑。另一个问题是参考设计中的耦合电路能应用于120V的直流载波电路吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
首先关于电阻值得问题,SBOA130A中2kΩ有误,请以datasheet(SBOS531D)中20kΩ为准。
这里的20kΩ,是因为AFE031内部功率运放的输入阻抗是20k。
对于120V的直流载波,参考设计中的耦合电路是ok的。但是需要注意的是:C18的耐压值需要高于最大的bus电压,还要加一些margin;另外可能还要考虑DC源的阻抗问题。