This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我用OPA333放大器做同相放大,要求输入直流电压信号为0时输出0.5伏,输入5mv时输出1V,按照下面的电路不正确,请问是什么问题?
图片错,R1是2M
你的IN+是输入?按照你目前电路,同相端输入5mv的时候,反相端也是5 mV,能放大输出1V吗?你目前输入0V及5mV,输出分别是多少?
输出几乎都为零,请问能分析具体点吗?谢谢!我是按ti书上介绍的放大电路
1、你再看看你的电路图及你参考的电路图,按照你目前的电路图输入为0的时候,输出应该为负,但由于供电是单电源,因此只能输出0V,而输入是5mV的时候,两个信号相等,输出也是零。
2、你只需要输入0V输出0.5V,输入5mV输出1V这两个点吗?没有别的要求吗?如果是,可以帮你改一下电路试试。
您好,非常感谢您的答复,要求是输入0~5mv,输出0.5~1V,请问这个怎么改呢?我感觉偏置应该加在同相端
上网搜索了一下没有找到OPA333的资料,感觉R1用2M的电阻太大了,可也没想到太好的方法,你按照下面的图试验一下看看输出如何:
R21和R24共同端不用接地?如果接,上面的电路只是阻抗匹配哦
要接地,我忘了画,不知道你说的“只是阻抗匹配”是什么意思