This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA128: INA128+同相跟随器电压输出不正常

Part Number: INA128

电路图如下,运放供电±12V,不接输入时测得Vout=-8.7v,请问电路是否有问题?谢谢!

  • 您好,电路+-12V供电没问题。Gain=1, pin1和pin8之间不接电阻,断路是没问题的。

    首先不建议运放的输入端悬空处理,输出很容易达到饱和或者不确定状态,增加功耗。

    其次对于INA128,需要注意使其工作在线性范围内的输入共模电压范围,建议使用Analog Engineer's Calculator这个工具帮助设计。

    下面是+-12V供电,Gain=1,Vref=0V条件下,Vin的最大最小输入范围。 使用时确保输入电压在这个范围内,才能使得INA128工作在线性范围i内:

  • 谢谢您的回复,问题已解决,确实是运放输入端悬空引起的饱和,在输入端与地之间加入电阻输出正常了。

    也感谢您推荐的设计工具!