Other Parts Discussed in Thread: LM833,

输入是10mv 1k—100k的正弦波,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
OPA2683是电流反馈型运放,它比电压反馈型运放需要多注意一些事项,如果使用LM833没问题,我想应该是其反向输入管脚的寄生电容太大造成的。对于任何电流反馈运算放大器来说,保持反向输入电容较低始终是非常重要的,但对于OPA2683则是非常重要的。 超过2pF的外部布局电容将开始达到频率响应峰值。 通过增加反馈电阻值,可以降低峰值,但从噪声和动态范围角度来看,最好保持低电容。 反相节点(> 5pF)上极高的寄生电容值可能导致输入级振荡,无法通过反馈元件调整进行过滤。
因此,您尝试增加反馈电阻R17到1.2K,看输出是否还振荡?
下面是datasheet 19页右半部分中间处的截图: