This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL084B: 输入的260Khz 1V的正玄波输出变成三角波是什么原因造成的?

Part Number: TL084B

您好:使用TL084C设计的一个260KHZ的放大电路,原理图和3个采样点波形如下图;运放的电源是24V。

     问题1) 设计的3倍放大,经过TL084B运放后,没有放大;

   问题2) 经过运放后,波形是三角波,正常的应该是正玄波才对。

测量点1波形

测量点2波形

测量点3波形