Part Number: XTR110
Other Parts Discussed in Thread: XTR111, XTR300
准备设计个电路:实现电压-电流转换,输入0~10V,输出对应-200mA ~ +200mA,
本来XTR110很合适,但我需要温度-40~+85的芯片,XTR110对用的工业级芯片已停产,
所以有什么更好的方案或芯片推荐?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,XTR300和XTR111是XTR110的相似产品,但是它们的工作方式和XTR110是不同的,不像XTR110 那样增益是可以通过调节外部电阻器设置的,所以XTR300和XTR111不能像XTR110 那样更改范围。
XTR110工业级芯片现在处于NRND状态,不再推荐新的设计,但是还未停产,不知您是否需要量产,如果少量应用的话,可以联系下供应商。
如果新设计用于量产的话,为了确保能正常供货的话,可以考虑替换,但是目前看来没有能直接替代XTR110,功能完全相同的器件。
这个是关于产品寿命和供货连续性的承诺,您可以参考下:
https://www.ti.com.cn/zh-cn/support-quality/quality-policies-procedures/product-life-cycle.html