This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM358: 应用问题

Part Number: LM358


目前LM358BA有如下技术问题,请帮忙看一下,谢谢!

    1、运放的一致性不好,是不是主要看失调电压(input offset voltage),还有其他参数吗?

          假如失调电压最大2mV,运放电路放大100倍;是不是输出偏差就会有0.2V?

    2、运放受温度影响,出现偏差,是不是因为 失调电压漂移(input offset voltage drift)?

    3、因为LM358BA的失调电压和失调电压的漂移会比LM358A好很多,是不是将LM358A 换成LM358BA ,一致性方面会有很大提高 ?

  • 您好,

    1、您是说的运放的哪方便性能一致性不好?如果说是各种原因造成的输出误差的话,那么主要看输入失调电压;影响输出误差的还有PSRR、CMRR、AOL、噪声等;

    假如失调电压最大2mV,运放电路放大100倍;是不是输出偏差就会有0.2V?

    是的,运放输出偏差最大会是0.2V。运放输出端的失调电压是运放输入失调电压乘以电路增益。

    2、是的,运放失调电压漂移占主要影响,同时还有输入失调电流漂移;

    3、是的,LM358BA各方面性能都比LM358A好,造成的输出误差会小很多。