This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA657: TIA 闭环带宽, 滤波器,设计合理性

Part Number: OPA657
Other Parts Discussed in Thread: OPA656, OPA855

Hi All,

当前设计想放大几十nA到几uA的APD电流,带宽1MHz以上,

TIA级如下:

有如下问题:

1,带宽

OPA657 GBP 2300MHz >> OPA656 220MHz,

但在同样的条件下 (Rf = 1Mohm, Cf = 0.2pF) ,

对比OPA657和OPA656带宽反而是OPA656大,是寄生电容不同的差异吗?

右边为OPA657

2. 在仿真噪声的时候,为了提高增益,增加反馈电阻Rf (同时为了不减小带宽,将Cf减小), 噪声明显增加。对比信号增加的幅度,SNR并没有明显提高。

仿真结果在TIA输出端噪声(total)为2.53mV, TIA输出用RC一阶可以降到1.9mV, 用二阶Sallen-Key 可以降到1.27mV, 可以稍微提高信噪比,但是没看到有设计是加二阶有源滤波器的,是有什么不合理的地方吗?

        

3. 目前结构是OPA657+ Sallen-key滤波+单端转查分驱动ADC。对于几十nA到几uA的APD电流,带宽1MHz以上这样的设计需求有没有更合理的,SNR更高的方案?

谢谢!