This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2904: LM2904做交流信号放大,输出摆幅不到0V

Part Number: LM2904
Other Parts Discussed in Thread: TLV2171,

差分放大倍数1.1倍,偏置电压1.785V,输入-1.195V时,输出波谷削波,电平0.72V。运放替换为TLV2171后正常,输出摆幅能到0V。

  • 您好,可以看下LM2904的输出电压距离电压轨的情况,当Iout=50uA的时候,正压距离电压轨典型电压为1.35V,负压距离电压轨典型值为100mV,也就是说5V供电,Iout=50uA,输出为0.1V~3.65V。 当Iout=1mA的时候,输出正压距离电压轨为1.4V,输出负压距离电压轨为0.75V,因此5V供电,Iout=1mA,输出0.75V~3.6V,LM2904 不是轨到轨输出的运放,所以单电源5V供电,输出是达不到负压轨0V的。

    再来看下TLV2171,可以看下它的输出距离电压轨基本上在mV级别,当供电电压+-18V,RL=10Kohm的条件下,5V供电,输出为0.09~4.85。 很接近正负电压轨。所以这是您测试下来发现TLV2171 要比LM2904 输出范围广的原因

    综上,如果单电源供电,输出如果想达到0V,或者0V附近,建议您选择轨至轨输出的运放器件,我们有很多轨至轨输入,轨至轨输出或者轨至轨输入输出都可以的器件。

  • 您好,感谢回复,实际测试验证,将运放输出悬空后,低电平幅值仍然为0.7V左右,没有变化,这种是否符合规格,或者可能由哪些原因引起?

  • 您好,输入输出是否能达到电源轨是和运放的输入输出设计有关的,这个是运放自身的问题。 

    您看下这篇以前资深工程师总结的,针对 轨至轨输出的详细解释:

    运放参数的详细解释和分析-part22, 轨至轨(rail to rail)输出 - 放大器论坛 - 放大器 - E2ETm 设计支持 (ti.com)