Other Parts Discussed in Thread: OPA846, OPA391
Hi,
我在查看OPA392的手册时 https://www.ti.com.cn/cn/lit/ds/symlink/opa2392.pdf ,看到其开环特性曲线如下,初始相移是180°。困扰我的地方是:按照之前的认知,开环曲线的初始相移应该是0°。如果是180°的话,那输入一个超低频信号时,因为输出相对输入有180°相移,输出的正负岂不是反向了。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi Amy,
我能这么理解你的回答吗,
1、运放对不同频率信号的相移是不一样的,但对于直流信号的相移一定是0 ,也就是OPA391手册上给的幅频特性曲线0HZ时是180°,这并不是真实运放对信号的相移。
2、运放相移是进行运放稳定分析的一个关键,(如果初始相移就是180°,那这个系统就是二型系统,正常来说就不能用bode图来进行稳定性分析),那我是不是可以直接把整个开环幅频特性向下移动180°,让运放变为一个零型系统,
如图我对一个0HZ下相频为180°的稳定性仿真,相位裕度;180+37 = 217°(这明显不太合理),是不是我做仿真分析的时候直接把相移往下移动180°,这个时候的相位裕度:180+(-143) = 37°。
1、是的,这只是参照180°开始随着频率变化;这样方便看相位裕度,即离0°线有多远裕度就有多少;
2、不是初始相移就是180°,初始相移或者说初始相位是0°,它是几阶系统得看在频域范围内它有几个90°相移台阶,二个90°台阶就是二阶系统,二阶系统也可以用波特图分析;
可以直接下移180°从0°开始,但它该是几阶系统还是几阶系统不变;
如上所说,从180°开始变化,离0°线多远就有多少裕度;也就是说相移143°,离0°线37°,相位裕度就是37°;总的来说相移180°就不稳定了。