This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
感觉Gian并不等于12dB,仿真出来的Gain=-32dB左右,不知道为何,使用Multisum仿真时,情况基本一致,gain=0dB和gain=6dB 情况正确就是Gain=12时是错误的,不知道为何
我算了下增益应该是3即275/(54.9+34)约为3;
在单电源供电下输入共模电压范围与增益设置有关,在±2.5V供电时,输入共模电压范围典型值是±1.3V,最小是±1V,因此在单电源5V供电时,输入共模电压最小是1.5V ~3.5V,我在仿真电路中测量输入共模电压是不满足要求的,我想可能是这个原因造成的。
1.您可以提供下使用单电源供电运增益Gain=12dB的仿真文件吗?我还是没弄出来。
2.并且关于增益 手册提供的计算方式如下,并且按照手册提供的阻值,计算Gian=0 gain=6 gain=12 计算值是对的
您好,很抱歉回复这么晚。
上述table1表格中的增益应该指的是datasheet中figure 45 如下截图中,输出与“Av,RIN”节点处信号幅值的增益,即输入信号不是指VS而是指下面截图红色圈内节点信号。这样对于输入信号VS的增益就是表格中的增益除以2,因为Rs, Rt 和 Rin形成的1/2分压。这样12dB仿真结果应该是6dB,与仿真输出一致。