This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA226-Q1: INA226AQDGSRQ1

Part Number: INA226-Q1
Other Parts Discussed in Thread: INA226

IN226 Rshunt spec里使用的是2mΩ,因为Rshunt不同,对应到INA226里应该会有不同的配置,比如1mΩ, 或者2mΩ,IN采样的电压是不同的,具体资料在哪里。谢谢

  • 您好,您应该指的配置寄存器0x00h。这个寄存器的配置控制着器件的操作模式。 您看下手册的7.6.1部分的介绍,是不是您这边想要的资料?

  • 看下来应该是7.6.2,不知道我理解的对不对。

    7.6.2 根据采样电阻两端的电压换算成寄存器01H的值,而读取的值需要处理器再进行换算一次,用2mΩ和1mΩ,读取的电压不一样,但实际电流是一样的,假如用2mΩ读取40mv,1mΩ读取20mv,寄存器的值是不一样的,但是采样电阻已知,就可以计算出电流,不知道我这样理解对不对。期待您的回复。

  • 您好,是的,您的理解是对的,不同的采样电阻得到的Vshunt电压是不同的,7.6.2部分的只读寄存器01h存储的是shunt电压,如何通过Vshunt电压得到的这个寄存器的值。并且以Vshunt=80mV为例介绍的如何得到的寄存器的值。