This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1通道为运放输出电压,2通道的电流在采样电阻上的电压通过运放放大得到2通道的电压
您好,
感谢您对TI产品的关注!OPA365供电电压是多少?输入的直流电流是多少?您可以附上测试的电路图吗
VE和VB都是3.4V
采样电阻是哪一个?采样电阻值是多少?流过的直流电流是多少呢
采样电阻是0.001欧,电流5A左右
您是低侧测量还是高侧测量?您可以附上被测回路吗?因为我看不出输入的共模电压是多少?
下管电阻采样
看您被测回路应该带有开关信号,使得输出端有很高的过冲毛刺。
J12是怎样与上图OPA365连接的?根据您的描述,我简单搭建了如下仿真电路,整体电路结构不知道是否与您的电路有出入?
下图中因为同向输入端的直流偏置,输出端有3.4V的直流偏置。采样电阻电压是反向放大-16倍,因此输出应该是3.4V-0.005*16=3.32V.
您可以将2通道,采样电阻电压每格表示的幅值调小一些吗?
您可以同时测量下供电电压VE和VB的电压波形吗?