压控恒流输出电路,如下:
如 LOAD的阻值在500欧到5K欧之间变动时,输出电流会明显变化。
请推荐,在输入为0到3V间变化,输出能恒定输出500uA到5mA,负载在500到5K欧变动时。输出电流波动不大的电路。
输出端电源在30V以内。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
我认为您可以参考下面参考设计来设计您的电路:
https://www.ti.com/tool/TIPD102
TIPD102 用户指南:https://www.ti.com/lit/pdf/slau502
下面链接电流源电路希望对您有帮助:
您的意思是说运放使用单电源供电吗?如果信号是正负双极性信号,即使使用单电源供电,也是需要提供偏置电压电源的,以使负信号可以被正确的偏置。
很抱歉,没有单电源供电的参考设计,下面链接中文档的第4章有一些电路的基本偏置方法,您可以参考: