Part Number: OPA847




如图信号通过SMA接口送到虚拟采集卡测量,带有很大的高频噪声如图1,此时用一个镊子如图4按在SMA的信号脚上,噪声消失如图2、3; 镊子的尖头和手握的部分并不导通(有绝缘涂层);若戴着手套操作则无法去除效果消失;将镊子换成一段杜邦线,一头连接SMA信号脚一头用手握住也可。不知到这个时什么原因;电路采用OPA847高速运放,反向比例放大电路。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OPA847




如图信号通过SMA接口送到虚拟采集卡测量,带有很大的高频噪声如图1,此时用一个镊子如图4按在SMA的信号脚上,噪声消失如图2、3; 镊子的尖头和手握的部分并不导通(有绝缘涂层);若戴着手套操作则无法去除效果消失;将镊子换成一段杜邦线,一头连接SMA信号脚一头用手握住也可。不知到这个时什么原因;电路采用OPA847高速运放,反向比例放大电路。
电路中其他节点信号也存在干扰。
下图1到图4为输入频率2k,VPP分别等于50mv,140mv,200mv,300mv正弦波对应的输出波形;比例运放的电路原理图如最后图所示。电源滤波采用0.1nf并100pf的滤波电容,原理图中没有画出。图5为输入90mv时,输入与输出波形(黄色是输入),图6是用镊子碰触输出后的输出波形(,梦中情波)。这个干扰看来是在板子上电后输入端就有的(注意不是信号源本身就有的,关闭电源,输出波形与输入波形差不多)。增大频率,图7为输入11kHz时的输出波形,感觉频率变高了,增益变得还更大了。将输入电容C3用导线短路后,输出为峰峰值为0,但是直流=4V左右。?不知道电路问题出在哪里,为什么会出现干扰,以及怎样消除这个干扰