This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
我们在使用LM2903PWR近期出现异常,异常情况如下:比较器输出异常,在上电过程中不能正常拉低,时好时坏。
此电路用于交流掉电检测,在生产中发现LM2903输入-0.63V时,输出引脚没有正常翻转,具体看PWR_DET的示波器图。同时正常的LM2903输入测量为-0.66V,输出是正常拉低的。
您好,
VCC电压是多少?看您加了迟滞电压,设置的VL和VH是多少?
所附输出波形对应的输入波形是怎样的?是否可以将输入信号和输出信号显示在同一示波器屏幕中?
上面图片可以看清每格代表的幅值,但是格子看不清,因此不能看出信号幅值。您可以上传一个清晰的图片吗?我想具体看下每个节点的信号幅值。
看下面电气表格截图,在单电源供电时,其输入电压范围是0V~VCC-2V,因此VCC是3.3V时,输入范围是0~1.3V,不确定ch3 P1点信号幅值是否满足运放要求。
看上面图片中,CH3(P1节点)红色波形示波器后半部分已经是负电压值,如上所述,在LM2903单电源3.3V供电时,其输入范围是0~1.3V,最小值是0V,不能是负值电压输入。LM2903的pin3红色波形已超出了这个范围,LM2903很可能会损坏。