This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA735: OPA735加OPA333

Part Number: OPA735

我要测试一下我的运放组的工作状态。电路图如下:

现在的电路是:当输入信号VG16.01V慢慢变化到7.22V时。输出电压Vout138.16mV变化到0.8745V

但是,我不知道这个变化是否是线性的。我需要这个变化是线性的,起码也是接近线性变化。我该怎样操作?

我现在要调整参数,使得当输入信号VG1从6.01V慢慢变化到7.22V时。输出电压Vout从200mV变化到1V。并且,要求当输入信号VG1从7.06V慢慢变化到7.22V时。 输出电压Vout的变化必须是接近线性变化的。我想知道我该怎样用TINA TI去仿真?怎样设置那个输入信号VG1才能达到我的目的。因为这个电压源好像只能从0V设置到指定的电压值,不能从一个指定的电压值(6.01V)设置到另一个指定的电压值(7.22V)。请赐教!