This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助: 高电压运放OPA454 的用法

Other Parts Discussed in Thread: OPA454

网友 dalong168  在 21ICBBS  TI 模拟技术论坛询问以下问题.

http://bbs.21ic.com/icview-586411-1-1.html

OPA454 的Status Flag 的作用,和E/D、E/DCom的用法,由于水平有限,数据手册没看明白,恳求赐教

  • Status Flag 这个引脚是过温或过流的标志位,如果结温过高,会拉高,如果回复到正常操作状态,会将此引脚拉低,它的架构为开漏输出,可通过一1Mohm电阻上拉到V+。

  • Enable/Disable pin是指的输出引脚enable和disable,即使将输出disable掉,也不会对输入信号有干扰,这样既节省了功耗也保护了负载,Enable/Disable pin 和Enable/Disable Common引脚构成了一个回路方便和外围低压逻辑电路连接。如果将Enable/Disable Common悬空,那么可被内部10uA的电流源拉到负电压轨,如果Enable/Disable pin悬空,那么Enable/Disable电压在Enable/Disable pin common 2V以上,您可以按照datasheet Figure67中将E/D com pin 接地,E/D pin通过一1Mohn电阻上拉到V+使得E/D电平时钟保持在OPA454 shut down门限电平之上