如下图,我司逆变器上面用到一个运放,TI的LM2904AVQDRG4
电源±15V供电时,产生的参考电压为1V和2V,没有任何问题
现在当电源改为±12V供电时,运放输入电压为1V和2V,输出电压变成了0.5V和1V,这是什么原因呢?
我把运放换成TL082BCDR,电路工作正常,运放输出1V和2V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,在您的应用中,使用LM2904作为电压跟随。如果+-12V供电,输入1V或2V是没问题的,符合它的输入共模电压范围。
在靠近LM2904的输入端,测量1V和2V电压是正常的是吗?然后输出发现电压变为0.5V和1V,电压减半是吗?
直接单位跟随,没有任何分压电路,并且是直流信号,输出幅值减半,肯定是不正常的。
有尝试在+-12V供电情况下,比如正弦波或者其他信号,输出正常吗?
您在哪里购买的芯片?