This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA320: 跨阻放大器中偏置电压对光电二极管的影响

Part Number: OPA320

在TI提供的Photodiode amplifier circuit,跨阻放大器电路,如下:

TIPD176:1 MHz, Single-Supply, Photodiode Amplifier Reference Design

为了把Photodiode 输出动态范围最大,Vb需要尽可能小(上文中设置为了100mV);但是Vb小了之后,也既是Photodiode加的偏置电压变小,

这会影响Photodiode光电检测的灵敏度吗?

对这个电路及Photodiode 特性熟悉的牛人,烦请帮忙释疑,感谢!

  • 您好,抱歉,我会尽快看下您的问题。

  • 抱歉回复晚了,不会影响光电二极管的灵敏度,Vb这里只是为了抬高Ipd*R1的电压,防止输出在负压轨饱和,虽然OPA320 是轨至轨输入输出,但是可以看到它的输出距离电压轨也有最大45mV的幅值(不同负载不同的输出范围),也就是说输出不能达到GND电压,最低电压也是比如10mV,达不到绝对0V。

    因此这里设置Vb在100mV能保证输出不会导致饱和。