当PEAKDET-OUT输出的电压曲线为蓝色曲线且Q12关闭、NSAC-Out输入为零时,为什么运放输出值为黄色的直流曲线??如果Q12开启时对整个电路有什么影响???
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
当PEAKDET-OUT输出的电压曲线为蓝色曲线且Q12关闭、NSAC-Out输入为零时,为什么运放输出值为黄色的直流曲线??如果Q12开启时对整个电路有什么影响???
您好,
Q12关闭、
Q12关闭是指Q12截止吗?如果是的话,为排除Q12没有完全截止您可以焊掉Q12吗?
NSAC-Out输入为零时
这里输入为零是指NSAC-Out接地吗?
供电电压V+和V-是多少?
PEAKDET-OUT输入信号幅值大概是±9mV?输入信号频率是多少?
R38电阻是多少?我想用TINA仿真一下
您是使用的TI的OP27吗?因为我查看TI的型号中没有后缀是G的;
PEAKDET-OUT的信号频率是多少?
我想可能是流过积分电容的电流太小的缘故,看OP27G 参数输入失调电流典型值是12nA,使得起作用的主要成分是输入失调电流,建议降低R57电阻调节电容积分电流。
ADI的产品建议咨询ADI的技术支持,这里是TI E2E论坛,请谅解。