This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA548: OPA548高温上电大电流

Part Number: OPA548


之前的OPA548的上电大电流问题,贵司最后的回复说是发生了热关断,根据手册说明可以知道,当发生热关断时不会有输出,而且ES的引脚电压会降低。但是我实际测试结果是当发生上电大电流时输出还会有电压值,但是电压值不准确,而且ES的电压没有降低,反而升高了。如图: 而且在高温上电都是在位置一段时间后才上电,可以保证器件在上电之前为高温的环境温度(90°C)

  • 补充相同测试项常温下得测试结果: ,为什么输出的电流测试结果在 常温和高温会有这么大的区别?

  • 您好,

    图片中的OUT-I和OUT-V是指哪里的信号?负载是什么?12V是指单电源供电电压吗?您可以附上测试所使用的电路图吗?

    图中仅有每格代表的幅值,但是没有显示出网格,因此看不出波形幅值。测试波形中您可以将每个波形的基准点和网格显示出来吗?这样我可以看出每个波形的幅值变化;