This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA548: OPA548上电后出现异常电压问题

Part Number: OPA548


设计电路如图所示:

12V(限流0.1A)和-1V(限流0.1A)使用直流电源供电,常温下上电后测试结果如下:

其中:

OUT-I为原理图中R7处改为线缆测试的电流;

ES为OPA548的ES输出;

OUT-V为原理图中C9处测试的电压值,正长应该一直为0V‘

12V-V为正电源的供电电压,在原理图中12V测试点处测得;

12V-I为正电源的电流,

-1V-V为负电源的供电电压,在原理图中-1V测试点出测得。

看测试结果一切正常。

12V(限流0.5A,限流0.1会把正电源供电拉下来)和-1V(限流0.1A)使用直流电源供电,高温85°C下上电后测试结果如下:

测试项和常温相同,但是此时发现输出会有一个异常的电压,而且正电源供电限流必须调整为0.5A以上,图片为调整0.5A限流后的测试结果。

想知道高温发生此异常电压现象的具体原因?