This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA388: 同向输入端大接地电阻的取值

Part Number: OPA388


 在模拟电路书上看到同相放大电路对交流信号进行放大时,需要为输入电路到地的回路,如上图所示,请问各位大佬,上图中R1的作用和原理是什么,阻值如何确定呢?

  • 您好,

    是的,交流耦合输入时要为运放的输入偏置电流提供DC路径。输入偏置电流会给耦合电容C1充电,直到超过运放的输入电压范围,这个过程很慢,但长时间工作后会使运放输出异常,因此需要一个直流路径将电容上的能量泄放出去,这就是R1的作用。

    输入耦合电容C1和对地电阻R1形成了高通滤波器,根据1/(2πRC)选择的R1首先要满足输入信号频率的要求;电阻也不能太大,因为这个电阻会将输入偏置电流转换为输入偏置电压,电阻越大形成的偏置电压也就越大,另外也要考虑电阻值越大引入的噪声越大,因此也不能选太大的值。