This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
OPA354 spec中 8.3.7 Capacitive Load and Stability章节说明了运放外接容性负载对其稳定性的影响以及改善稳定性的方法。
单位增益配置中的运算放大器最容易受到电容负载的影响,图13如下截图,可以看出在单位增益下不同容性负载的频率影响。减小大电容负载的振铃的方法是在运放输出端串联一个隔离电阻RS,RS取值见如下截图14,以及频率响应下面截图图15。
另外需要注意的是 如果存在与电容负载并行的电阻负载,如下截图所示,RS会创建分压器。这种电压分配会在输出端引入直流误差,并略微降低输出摆动。例如,当RL = 10 kΩ 且RS = 20 Ω 时,输出处的误差约为0.2%。
没有加RS,也没有接负载电容,测试条件在spec中 7.8 Typical Characteristics 章节 典型特性曲线最上方,每一页都有,即 at TA = 25°C, VS = 5 V, G = +1, RF = 0 Ω, RL = 1 kΩ, and connected to VS / 2。