我在用VCA810做程控放大器,正相输入端做了个调零电路,反相输入端输入信号,Vc 端用 DAC7512产生控制电压,经过反相放大器接到Vc,现在是DA可以产生电压,输入到Vc是 -1 ~ -2 的 负电压,但是当接入控制电压后,供电电压端电流会增大到40mA,输出端什么都产生不出来,请问为什么会这样,我用TINA仿真时都是正确的 下面是原理图
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
按照手册11页图30的接法先验证VCA810是否正常。
1. 控制电压从稳压电源给,拆R7,R8
2. 调零电路除R4外全拆,改R4=25欧姆
3. 改R2=0欧姆,保证信号源的内阻是50欧姆。
4. OPA656断掉,或者power dwon,使其不影响VCA810。
谢谢您的回答,我想用OPA656做一个跟随器,因为后级还要接功放电路,要放大10倍的,所以在VCA810后接的OPA656,这样不可以吗?
不好意思过了这么久,供电电压是指从电源产生的电压,输入是有函数信号发生器产生的1V,中频正弦波
建议先断开其他模块,调通VCA810后再把其他模块一个一个挂上,看看是哪个模块挂上之后功能不正常的。
VCA810后接OPA656,应该没问题。不过我拿不准中间要不要端接,你可以看到656手册一些典型应用电路图,输入都是要考虑端接的,而810的手册里输出就没有端接方面的内容。可以试试把R6改成50欧姆,同时在656输入端端接一个50欧姆到地。实际调试时,因为810肯定会有输出阻抗,所以通路上的50欧姆应该是往小调,以达到阻抗匹配。